Search FAQs
How to know the absence of x80 IO in local M580 rack when it is configured as Device DDT ?
1.Issue
How to know the absence of x80 IO in local M580 rack when it is configured as Device DDT ?2.Environment
M580 series ,X80
3.Resolution
The detail diagnostics status of x80 IO could be accessed by implementing READ_STS_MX.
Here are two samples to get status for digital and analog modules.
When COM_FLT is set to 1 ,it means the module could not be detected by CPU and module would be absent in the rack.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: