{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you explain how VIP3xx relay work with VAP6 test box ?
Issue :
VIP3xx relay work with VAP6 test box

Environment/Product line:
VIP 300 relays

Resolution :
Basic concept is any trip testing with the VIP300 should be done with the VAP6 test box
and VIP300 uses a MITOP output to send tripping commands.

VIP300 MITOP output is a capacitor. This is supposed to be connected to a small coil which has enough energy to trigger a small mechanical switch which then triggers a CB Trip operation.
The MITOP output should not be used as a Trip Contact like what you would find on a Sepam 20 relay (example :O1 output)

Since it is a microprocessor-based relay, testing with a VAP6 box should be sufficient. As long as the relay trips when you follow the procedure in the manual,
there is not really any need to perform "tripping delay" tests.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: