{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ION9000 - PTP time sync not work. Nothing happens after clicking the sync button in ION Setup

Environment:
ION9000 PTP time sync
-------------------------------------------------------------
Issue:
Time sync does not work. Nothing happens after clicking the sync button in ION Setup.
-------------------------------------------------------------
Cause:
In the PTP server, the Network Protocol setting needs to be IPv4. With this set to IEE 802.3, time sync does not work for the ION9000 meter.
PTP can work on layer 2 (Ethernet 802.3) or layer 4 (IPv4, IPV6). In ION9000 the implementation only supports layer 4. 
image.png
-------------------------------------------------------------
Proposed Solution:
Change the PTP Network Protocol to IPv4.
There is no workaround as of now. If the customer wants this feature, this will be a feature request that needs to do through sales channels.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.