{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM5111 - Why LED energy pulsing configuration is not available
PM5111 meter is MID compliant. As per the requirement of the MID standard, the energy pulsing is fixed based on the PT and CT secondary values. So, the user is not allowed to configure the energy pulsing for LED in MID references. This is why the LED configuration option is not available in the PM5111 meter.

Schneider Electric Saudi Arabia