Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
In Ecodial 4.9.4 NL , How does panel communication happens when we select ‘ NONE , BMS and CLOUD ‘ options as supervisory ?
1. When  we select option as “ NONE” as the supervisory type then No solution found will gateway will be proposed by Ecodial.
 
2. When  “ BMS” is selected as the supervisory type and switchboard type is selected as “ Prisma G “ then “EcoStruxure Panel Server Universal gateway” will propose by Ecodial.
 
3. When “ CLOUD”  is selected as the supervisory type and switch board type is  selected as “ Prisma G “ then “ PrismaSet Wireless Panel Server “will propose by Ecodial.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: