{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 40 Energy Counter values (MWh, MVARh, etc...): can I set or configure the scaling or precision for these energy values?
No.  For the Sepam 40 Energy measurements such as MWh (Active Energy) and MVARh (Reactive Energy), the scaling or precision both on the front display and also the values retrieved via Remote Communication cannot be set.

For example, if you read the Energy values by Modbus, they are returned in units of 100kWh or 100kVARh.  This is not configurable in the relay.

On the front display, the values are displayed in units of MWh or MVARh, with a resolution of 0.1MWh or 0.1MVARh.

AEDL3

Schneider Electric Saudi Arabia