{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the functions of iATL24, iACT24, RCA when connected to Smartlink EL B?

iATL24 is used with iTL to integrate impulse relay control and indication into Smartlink ELEC
iACT24 is used with iCT to integrate contactor control and indication into Smartlink ELEC
RCA is used to control iC60 Circuit Breaker and reclose it in case of fault tripping.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.