{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement external reset button for Class 8536 Type SAG, Type SBG, or Type SCG starter?
Issue:
What is the replacement external overload reset button on the 8536 Type S starters?

Product line:
NEMA starter, 8536 Type SAG SBG SCG (, sizes 00, 0, 1)

Environment:
NEMA and Definite Purpose Contactors and Starters

Cause:
Replacement parts

Resolution:
Part number for the external reset bar/button is 9066SC1.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: