{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where are Rectivar DC drives supported?

Issue:
Support for Reactivar DC Drives.


Product Line:
All


Environment:
All


Cause:
Technical assistance for Rectivar Drives


Resolution:

These devices were never commercialized in the United States. Therefore there is little / no expertise or support available for them.


Users should also go back to their point of purchase for help. For example, if the drive came into the country on an OEM`s equipment, the caller should contact the OEM. If the unit was sold by the Industrial Automation Team as part of a system, the user should contact them.

Additionally, if the unit can be sent in for repair / evaluation, the device can be returned to the Repair Depot in Greensboro, NC. They offer limited repairs on these devices.

Schneider Electric Saudi Arabia

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: