{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the amount of current imbalance required to trip the feature unit 9065 solid state overload relay?

Issue:
When will a Solid State Overload trip when there is current Imbalance

Product Line:
NEMA and Definite Purpose Contactors and Starter

Environment:
9065 Solid State Overload Relay

Resolution:
The unit is guaranteed to trip within 3 seconds at 25% phase current imbalance. It will start tripping at +/- 17% imbalance.

Schneider Electric Saudi Arabia