Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In a 3 phase system, why does the meter still show voltage reading on one of the phases even after breaking the phase circuit?
Issue:
Testing phase loss on a meter doesn't result in a null voltage reading.

Environmnet:
EasyLogic Series Power Meters
PowerLogic Series Power Meters

Resolution:
The voltage seen is what we call "phantom voltage", its a known phenomenon with all high impedance power meters. These phantom voltages are normal artifacts of the design and should not pose any safety concerns to the end user.

In some cases it'll probably disappear by power cycling the meter. Most power meters are not designed to monitor phase loss, as it'll always assume the presence of the 3 phases and the neutral, depending on your parameters setup. External devices are used to detect such occurrences, like phase control relays.

Schneider Electric Saudi Arabia

Attachment(s)
Phantom Voltage White Paper 7EN52-0331-01.pdf [241.22 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre