{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Double click do not work Control Expert session is running on an extended monitors
If you have 3 additional displays configured as extended monitors, the double click function does not work on the extended monitor.  This occurs when Control Expert session is running on the extended monitor.

This issue has been fixed in Control Expert 15.   To resolve the issue, you need to upgrade to Control Expert 15 as a minimum.

Schneider Electric Saudi Arabia