{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Settings Required to Connect Gurux DLMS to ION meters

Issue
User unable to connect to ION meter via DLMS
_____________________________________________________________

Product Line
ION9000
ION8650
ION8800
ION7400
_____________________________________________________________

Environment
Gurux DLMS Director
_____________________________________________________________

Solution
Different software may require different settings. The settings below are for Gurux DLMS Director. Values are in hex. For example Physical server 64 is decimal 100.

Start Protocol: DLMS
Logical Name Reference: Checked
Authentication: None
Client address 10
Physical Server 64
Host Name: IP address of meter
Port: Port defined on the meter, default is 4059
Protocol: Tcp
Use Serial port through ethernet: Checked
_____________________________________________________________

Schneider Electric Saudi Arabia