{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Connexium log file be used to troubleshoot network issue.

TCSESM Connexium Switch logs usually do not provide enough information to troubleshoot an issue.  Typically, assistance from Belden or a Google search the message shown in the log can help understand it's meaning.  However, there is not enough information in the logs to help troubleshoot an issue with a Ethernet module.

We normally rely on the network topology diagram and Wireshark traces of the Ethernet traffic going to and from the Ethernet port on the module. Usually, we request a Wireshark trace of the Ethernet traffic before, during and after the issue occurs. The trace should be taken in promiscuous mode using either a hub or mirrored port on a managed switch.

Schneider Electric Saudi Arabia