Search FAQs
Masterpact MTZ: Components needed to locally operate breaker via smartphone app
Issue: Local operation via phone app capability was not ordered from the factory. Need to field modify.
Product Line: Circuit Breakers
Environment: Masterpact MTZ
Resolution: to field modify, the following components are required. Some of these parts may already be installed.
![image.png](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009mI7wQAE&oid=00DA0000000abSmMAI)
Then declare accessories
![image.png](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009mI7xQAE&oid=00DA0000000abSmMAI)
Product Line: Circuit Breakers
Environment: Masterpact MTZ
Resolution: to field modify, the following components are required. Some of these parts may already be installed.
- Mobile App – EcoStruxure Power Device
- Masterpact Operation Assistant Digital Module LV850005
- XF-Com, MX-Com coils, part numbers vary based on voltage.
- Spring Charging Motor, part numbers vary based on voltage.
- Isolation Module LV850056SP
- Isolation Module to coils communication cables MTZ1: LV833118SP, MTZ2/MTZ3: LV847904SP
- MX-Com cable needs to be plugged into the MX1 location on Isolation module, not MX2.
- Coils properly wired, C3 and A3 continuously powered. C2 and A2 are only needed for push button operation.
- Accessories Declared in the Control Unit via EPC, click the accessory pencil
Then declare accessories
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: