{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where are the System SD Card and Data SD Card slots on the HMIG3U?
Issue
I would like to find where the SD Card slots are on the HMIG3U, for both the System Card and Data Logging card.

Product Line
Harmony HMIG3U (HMIGTU Family)

Environment
Physical HMI

Resolution

In each of the photos below, the top of the photo is the 'back' of the HMIG3U (where you can see the COM port and Ethernet port labels). The bottom of the photo is where the screen is mounted.
With larger screens, the HMIG3U needs to be detached from the screen to be able to open and access the SD CARD slot flap.
Location

SD

Part numbers are as follows:
Replacement 1GB System SD Card required for the HMI to function: HMIZSD1G
4GB SD Card for additional data logging (optional): HMIZSD4G

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: