{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Clarify the 'Normally Closed' and 'No Connection' pinouts for a 140DRC83000
Early Quantum IO Manual nomenclature for the 140DRC83000 was not clear when defining 'Normally Closed' and 'Not Connected' pinouts.  The manual used the symbol N/C for both conditions which could lead to incorrect wiring and confusion.

Updated versions of the Quantum IO Manual (12/2018) for the 140DRC83000 connections are indicated by:
Normally Closed = N.C.
Not Connected = N/C
Normally Open = N.O

The following diagram clearly defines each pinout.

wiring pinout

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: