{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the Panel Server Support ION Protocol ?
Product Line
EcoStruxure Panel Servers

Environment
Panel Servers + ION Meters (ION7650, ION9000, ION8xxx, PM8000)

Question
Does the Panel Server support ION protocol ?
Link150 has an ION Pass Through service. Is it the same for the Panel Server ?

Answer
ION protocol will not be supported by the Panel Server.
Only the Modbus Map of the ION meters will be supported.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: