{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why are there two different current ratings given on the ATS22 soft starter?
Issue:
Why are there two different current ratings In and icL given on the ATS22 soft starter?

Product Line:
ATS22

Environment:
All

Cause:
Which is used to selection motor size.

Resolution:
-ICL is the current nominal of the starter, the starter is able to be through by this current continuously

-In is nominal current setting of the motor. In factory setting, the current In is the most common current of the motor issue of the NEC current table @ 460V . The control, limitation current are indexed on motor FLA.

You pick the soft starter bases on the IN ratings to match your motor FLA

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.