{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why all the LEDs of RM35JA32MW blinking during operation?
The position of the switch, and therefore the operating mode, is read by the product on energization.

If the switch is set to an unacceptable position, the product detects a fault, the output relay stays open, and the LEDs flash to signal the position error.

If the switch position is changed while the device is operating, all the LEDs flash, but the product continues to operate normally with the function selected at the time of energization preceding the change of position.

The LEDs return to their normal state if the switch is returned to the original position selected prior to the last energization.

Schneider Electric Saudi Arabia

Attachment(s)
Capture1.png [172.17 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: