{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NetBotz 750/755 "400 error" if not filling in identification fields fully
Issue:
NetBotz 750/755 "400 error" if not filling in identification fields fully

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755
Version 5.2.4 firmware and below

Cause:
If any of the identification fields are left blank when configuring Settings-->Identification on a NetBotz 750 or 755, a 400 error may appear

Resolution:
Be sure to fill each field with text and the error should not appear. It has also been seen where adding text, saving, then re-editing may allow for a blank field.

This issue is resolved in the NetBotz 5.3 release.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: