{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Network Shutdown – some VMs are not started for HyperFlex cluster
Issue:
PowerChute Network Shutdown – some VMs are not started for HyperFlex cluster

Products:
PowerChute Network Shutdown v4.4, v4.4.1

Environment:
PowerChute Network Shutdown configured with HyperFlex support with VMware as hypervisor

Cause:
After the HyperFlex cluster service has started, some VMs may still be in an inaccessible state when PowerChute attempts to power them on. When this happens, the power on attempt will be unsuccessful and these VMs are not re-attempted.

Solution:
Increase the Cluster Startup Duration in PowerChute to allow enough time for all VMs to become accessible in the inventory before VM start up occurs.

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.