Issue
"Configured" status is not displayed (checked or unchecked) in TGML for Cubicle 5 to Cubicle 16 for SMD (Switchgear Monitoring Device)

Product Line
PO2021 PSO2020 R2 CU1
Environment
PO2021 / PSO2020R2CU1 with webHMI application having SMD devices
Solution
"Configured" status is not displayed (checked or unchecked) in TGML for Cubicle 5 to Cubicle 16 for SMD (Switchgear Monitoring Device)
Product Line
PO2021 PSO2020 R2 CU1
Environment
PO2021 / PSO2020R2CU1 with webHMI application having SMD devices
Solution
- Close any open webHMI application in browser
- Stop IIS from IIS Manager
- Navigate to C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
- Take backup of "Thermal" Folder in v2021 folder and its sub-folders (C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021)
- Replace the attached (Related) TGML files in Thermal folder normally located at C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
- If your installation location is different, please make sure you replace these files in Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
- Start IIS Manager
- Open the TGML for SMD and verify the "Configured" Status visible for all Cubicles.
- If not able to view updated TGMLs , perform iisreset using Command Prompt (Required Administrator privileges).
Released for:Schneider Electric Saudi Arabia