I added Shutters to Shutter Group on the Free Locate Switch, but when I press the Free Locate Switch the shutters won't react
For the Shutters, you need to long-press on Free Locate Switch (>2s) to run the Shutters, with a short press you will then stop the movement of the Shutter blinds in the desired position.
Released for:Schneider Electric Saudi Arabia
Explore more
Product:
EKO07117
WDE002924
WDE002906
550D6001
EKO07116
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.