{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can TeSys Giga Relay be used along with TeSys D contactors (≤150A) ?

TeSys Giga overload relays can be used along with TeSys D contactors. However, they can’t be directly installed downstream to the contactor because the pitch between poles do not match. They can be individually installed with proper connection between them.

Note: There’s no coordination available for TeSys D contactors and LR9G relays

Schneider Electric Saudi Arabia