Search FAQs
How to interlock contactors in two different sizes of TeSys Giga contactors ?
TeSys Giga contactors can be interlocked with same ratings or with different ratings. The
various ratings have similar frame sizes and interlocking kits are defined based on the frame sizes.
![image.png](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H00000ARYRvQAP&oid=00DA0000000abSmMAI)
Note: Maximum 3 auxiliary contacts can be installed between 2 contactors with mechanical interlock kit.
various ratings have similar frame sizes and interlocking kits are defined based on the frame sizes.
Ratings | Frame size |
G115-G225 (115A-225A) | Frame 5 |
G265-G500 (265A-500A) | Frame 6 |
G630-G800 (630A-800A) | Frame 7 |
Note: Maximum 3 auxiliary contacts can be installed between 2 contactors with mechanical interlock kit.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: