{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is an S-Flex run contact wired?

Issue:

On which terminals are a run contact landed on the S-Flex?

Product Line:

S-Flex

Environment:

Design series E for models with bypass

All models without bypass

Cause:

Hardwiring a run contact

Resolution:

The S-Flex models without bypass use a dry run contact wired between terminals P24 and F. This is a 24Vdc circuit.

The S-Flex models with bypass use a dry run contact wired between terminal 5 and 6. This is a 120Vac circuit and controls Start/Stop when the HOA selector is in the AUTO position.

Schneider Electric Saudi Arabia