{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ATV320 showing tnF when turning on the drive
Issue:
Drive is showing tnF (autotune fault) when the drive is turned on

Product Line:
ATV320

Environment:
ATV320 all series

Cause:
ATV320 is showing tnF at the moment to turn on the drive.

Resolution: 
Confirm if motor is connected to the drive.
If motor is connected, there should be a problem with the feedback of the motor.
It will be important to double check the terminals, cables, and motors. If it is possible megger the motor.
If motor is not connected to the drive take a double look in the “Automatic Autotune” parameter. If this parameter is active the drive will be trying to get the feedback from the motor, but there is no motor to provide a feedback for doing the autotune of the motor.
Go to:
Conf-> FuLL > DRC-> ASY:
Aut [Automatic autotune]: select “no”
atv320 tnf
 

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.