{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why does my HMI return wrong object using modbus FC04 on a M580 CPU (OS3.1 and 3.2)?

description du problem
Historicaly, if an HMI wished to read a %MW or %M object, in a Premium CPU, the HMI was adressing a modbus request "FC04" to the CPU. If the number of %IW and %I configured in the CPU was equal to "0", the modbus server of the CPU accessed to %MW and %M area. => The modbus server of the CPU delivered %MW and %M.
If the number of %IW and %I configured in the CPU was not equal to "0", the modbus server of the CPU accessed to %IW and %I area. => The modbus server of the CPU delivered %IW and %I.

To avoid any migration problem from Premium to M580, we have kept the same rule on the PLC range M580.
The problem is that if a client select in CE15.0 a CPU BMEP58xx20 OS 3.0 or 3.1, the minimum value of %IW and %I has been change to a value different of "0". So the HMI received %I objects instead of %M.

image 2.jpg

by consequence the HMI doesn't get the expected object!
image1.jpg
This different behavior will be fixe in the next version of CE15.1.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: