{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to resolve SoMove/EcoStruxure Machine Expert/EcoStruxure Control Expert crash issue after TeSys island DTM Library is installed

Description of the Problem:

Customers using V2.2.2 of TeSys island DTM Library might experience SoMove/ESME/ESCE* crash when they install any other version of TeSys island DTM library and open SoMove/ESME/ESCE.

DTMs impacted:

TeSys island DTM library V2.2.2

Root Cause:

There is a bug in the TeSys island DTM library V2.2.2 installer which deregisters FDT DLL during uninstallation.
This causes SoMove/ESME/ESCE to crash.

Solution:

Note: Perform the following steps strictly in the order mentioned.
  1. Uninstall TeSys island DTM Library V2.2.2
  2. Install/Re-install the existing/new version of SoMove.
  3. If ESME/ESCE is installed on the machine and not SoMove, Install/Re-install ESME/ESCE. Alternatively, Install latest version of SoMove.
  4. Install latest TeSys island DTM Library.
*ESME - EcoStruxure Machine Expert
*ESCE - EcoStruxure Control Expert

Schneider Electric Saudi Arabia