Is the contact wear diagnosis LED only an indication or it will also affect the status (performance) of the contactor/ overload relay ?
Contact Wear Diagnosis (CWD) LED function is only for alarm purposes, to help customers for predictive maintenance and it doesn’t impact the normal functioning of the contactor or the overload relay.
Released for:Schneider Electric Saudi Arabia
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.