{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is cable memory function of TeSys Giga contactor ?
Cable memory function is enabled by an optional cable memory kit, to which the cables or busbars can be connected to the contactor. The cable memory kit is installed on both sides of the contactor, and the main power connections are connected to this kit. The contactor maintenance (replacement of control module or switching module) can be done without removing them and helps reducing downtimes.

Note: Advanced version contactors are always equipped with cable memory kit and it's an optional accessory for Standard version contactors.

image.png

Schneider Electric Saudi Arabia

What is cable memory function of TeSys Giga contactor ?
Cable memory function is enabled by an optional cable memory kit, to which the cables or busbars can be connected to the contactor. The cable memory kit is installed on both sides of the contactor, and the main power connections are connected to this kit. The contactor maintenance (replacement of control module or switching module) can be done without removing them and helps reducing downtimes.

Note: Advanced version contactors are always equipped with cable memory kit and it's an optional accessory for Standard version contactors.

image.png

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: