{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Control Expert 15 returns error 'mfc140u.dll is missing' when starting
Control Expert returns the error 'system error: mfc140u.dll is missing' when trying to start.

This error will occur if the mfc140u.dll file already exists on the PC and it is of a newer version when Control Expert is installed.  The 'mfc140u.dll' file is part of the 'Microsoft Visual C++ 20xx Redistributable ' libraries that gets installed during the Control Expert installation process.  Per Microsoft rules, a software installation is not allowed to overwrite an existing version of a Microsoft '.dll' with an older version.  This rule prevented the
proper installation of the required  'Microsoft Visual C++ 20xx Redistributable ' libraries.

image.png


The specific version 'mfc140u.dll' file is essential for the registration of other '.dll's that are included with Control Expert.  As a result of this, the error could also be accompanied with the following error:

image.png

To resolve the issue,
  • Rename the existing .'mfc140u.dll' file.
  • Uninstall Control Expert.
  • Reboot the PC.
  • Reinstall Control Expert.

Schneider Electric Saudi Arabia