{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PME 2021 - KPI Report not saving the calculated data into the database

Product Line

Power Monitoring Expert 2021 - CU 1

_____________________________________________________________

Environment

Web Application - Reports

_____________________________________________________________

Issue

KPI Report not saving the calculated data into the database.

The following error message is logged into ION_Systemlog:

KPI Calculation Engine Failed. See system logs for details

"Could not load file or assembly 'MeasurementManager.Data, Version=1.0.0.0, Culture=neutral, PublicKeyToken=null' or one of its dependencies. The system cannot find the file specified."

_____________________________________________________________

Root Cause

The MeasurementManager.Data.dll file was missing from the system\ReportDataService\bin\

_____________________________________________________________

Proposed Solution

Make a copy of the MeasurementManager.Data.dll file located at system\bin and place it in the system\ReportDataService\bin folder

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: