{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMXNOM0200 with M580 INPUT_CHAR limitations

Issue

How many INPUT_CHAR blocks can be processed at the same time?

Product line

Control Expert, Modicon M580, Modicon X80

Resolution

The NOM uses XBUS and the M580 can only process 16 XBUS messages per scan. In addition, the BMXNOM0200 has a buffer that can only handle 16 INPUT_CHAR messages at a time. The limit is 16.

Schneider Electric Saudi Arabia