{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In Ecostruxure Operator Terminal Expert 3.2 SP1 how many devices can be added using a Modbus TCP driver?

Issue:

How many devices can be added on Ecostruxure Operator Terminal Expert 3.2 SP1 when using a Modbus TCP driver?

Product Line:

Ecostruxure Operator Terminal Expert 3.2 SP1, HMIST6, HMISTM6, HMIG3U, HMIG5U22, HMISTO735 and iPC.

Resolution:

The maximum number of devices that can be added under the Modbus TCP driver depends on the HMI model, as follows:

HMIST6 family: Up to 32 devices.

HMISTM6 family: Up to 32 devices.

HMIG3U/HMIG5U22: Up to 64 devices.

HMISTO735: Up to 16 devices.

iPC: Up to 64 devices.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: