undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to set IP address of a HMIGTO target when using Modbus USB Equipment connection in VJD 6.2 SP11?

In Vijeo Designer 6.2 SP11, we can't set HMIGTO IP address in the same network segment with a M340/M580 PLC when you try to connect the HMIGTO to the M340/M580 PLC via USB. As we know, the default IP address for M340/M580 PLC is 90.0.0.1, which we can't change. So we can't set the HMIGTO IP address as 90.0.0.<example>. Otherwise there will be no connection.

Schneider Electric Saudi Arabia

How to set IP address of a HMIGTO target when using Modbus USB Equipment connection in VJD 6.2 SP11?

In Vijeo Designer 6.2 SP11, we can't set HMIGTO IP address in the same network segment with a M340/M580 PLC when you try to connect the HMIGTO to the M340/M580 PLC via USB. As we know, the default IP address for M340/M580 PLC is 90.0.0.1, which we can't change. So we can't set the HMIGTO IP address as 90.0.0.<example>. Otherwise there will be no connection.

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top