{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power SCADA Operation (2020/2021) with OPCUA Driver v4.00.05.00000: OPCUA client not working for tags include Chinese characters
Issue
One issue related to PSO2020+CU1 as OPCUA client issue. with the newest OPC driver - OPCUA Driver v4.00.05.00000.
If the OPCUA server tags include Chinese characters, PSO can’t read the data and it will show bad.

We have replicated customer’s issue.


Also test with other OPC UA client and it can be read.


Environment
Power SCADA Operation (PSO) 2020 R2

EcoStruxure Power Operation (EPO) 2021
KEPServerEX 6
Matrikon OPC UA Explorer

Cause

Citect does not support Unicode tag address. It also does not support Unicode tag values, tag names, etc.

Resolution
For tag address/name you can only use standard ASCII characters (no special characters).

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: