{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMENOC03x1 and RSTP

Issue

Planning on using the BMENOC0301 or BMENOC0311 in a configuration where RSTP is not allowed and need to disable this feature.

Product line

Modicon M580, Control Expert

Resolution

As of June 14, 2023 (v2.21) there is no way to disable RSTP. If you need a port without RSTP you can use the service port. The service port of the BMENOC03x1 modules does not support RSTP.

Schneider Electric Saudi Arabia