{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How long will a NetBotz 750 / 755 store data or alerts?
Issue:
How long will a NetBotz 750 / 755 store data or alerts?

Product Line:
NetBotz version 5

Environment:
NBRK0750
NBWL0755

Cause:
NetBotz have a limited memory capacity and can not store alarms or data for an extended period of time.

Resolution:
NetBotz can store data and alarms for up to 96 hours. After that, the older data is purged. If you are using multiple cameras and capturing images on a constant basis, the NetBotz may have to purge it's information sooner. In such a configuration, it is recommended that you use StruxureWare Data Center Expert and it's surveillance option for image storage for a longer term. You can also simply send alarms to an e-mail and store them that way.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: