{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why the SNMP agent information are not anymore visible on BMENUA0100 module after a Control Expert migration ?
During the creation of a project in CE V14.1 or CE V14.0 with a BMENUA0100 module and SNMP agent has been configured.


During the migration from CE 14.0/14.1 to CE V15.0/CE15.0 SP1, the SNMP agent could disappear like the following screenshot:

In this case, we suggest you to contact the technical support in order to solve the problem.
This problem will be resolve in the next version of Control Expert CE v15.1

Product Line

Control Expert CE v14.0, CE v14.1, CE v15.0 and CE v15.0 SP1

Environment
BMENUA0100

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: