{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does triangle with exclamation mark on the Display for the iEM3000 represent?
Answer
Issue
What does triangle with exclamation mark on the Display for the iEM3000 represent?
_____________________________________________________________
Product Line
iEM3000 series meters
_____________________________________________________________
Environment
Power Monitoring Expert (PME)
ION Setup
Modbus mastering
_____________________________________________________________
Solution

The triangle icon will be displayed in iEM3255 if any acknowledged alarm is active.

Once the alarm is acknowledged, this will disappear.


Iem3255-Triangle icon-Final.jpg

Schneider Electric Saudi Arabia