{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which access point wifi or 4G router can be recommanded to work with Harmony STM6BOX (Gateway Box Model)?
The goal is this FAQ is to propose some recommented architectures using access point wifi / 4G to connect to Web Viewer

This article is applicable for HMIST6xx, HMISTM6B, HMISTM6BOX + EcoStruxure Operator Terminal Expert

Architecture 1: HMIST6/HMISTM6, HMISTM6BOX + Wifer TCSEGWB131W
Architecture STM +wifi
Architecture 2: HMIST6/HMISTM6, HMISTM6BOX + Router Wifi Teltonika RUT240
Architecture STM +wifi

Architecture 3: HMIST6/HMISTM6, HMISTM6BOX + Router 4GTeltonika RUT240 through EcoStruxure Secure Connect Advisor

secure connect

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: