{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

ION Setup unable to configure the logical circuits of EM4908E

Issue
Unable to configure logical devices for EM4908E in ION Setup V3.2

Product
ION Setup
EM4908E

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop). *

A) Close ION Setup and find the location where ION Setup is installed, typically C:\Program Files (x86)\Schneider Electric\ION Setup\
B) Open the folder "Tables"
C) Open the folder "EM4900"
D) Open the folder "EM4908E"
E) Backup the file "Setup.cfg", save to a safe location
F) Edit the Setup.cfg with a text editor program such as notepad
G) Search for "[Logical Meter Setup]" (without quotes) there are 2 lines in this section to update

FlexCircuits=24

and

Registers=24

H) Save changes
I) Open ION Setup and configure the logical circuits for EM4908E meter

Note that a future version of ION Setup will have updated values.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: