{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Part Number to unlock the WebViewer feature for Harmony HMIST6, HMISTM6, or iPC?
Issue
In order to unlock the WebViewer feature in the Harmony HMIST6, HMISTM6, or iPC what is part number of the License?
How is it unlocked on an iPC?

Product Line
Harmony HMIST6 (HMIST6200, HMIST6400, HMIST6500, HMIST6600, HMIST6700)
Harmony HMISTM6 (HMISTM6200, HMISTM6400)
Harmony HMISTM6BOX
EcoStruxure Operator Terminal Expert v3.2 SP1 and up

Environment
WebViewer feature for HMI for browsing from a PC

Resolution
For both the Harmony HMIST6 and HMISTM6 series HMIs, the license required to activate the WebViewer feature have the following Part Numbers:
HMIWRT001 - EOTE WebViewer keycode - 1 pc
HMIWRT010 - EOTE WebViewer keycode - 10 pcs
HMIWRT100 - EOTE WebViewer keycode - 100 pcs

Ordering the part number will give you a unique keycode that you enter in the HMI's Hardware Configuration screen in the section called "Web Viewer" at the bottom of the menu to unlock the feature on the hardware itself.

This feature requires EcoStruxure Operator Terminal Expert v3.2 SP1 or higher (programming software for Windows) as a minimum version to support the WebViewer Feature.

For Harmony HMIST6 (HMIST6200, HMIST6400, HMIST6500, HMIST6600, HMIST6700) or
Harmony HMISTM6 (HMISTM6200, HMISTM6400), you will need:

  1. Basic License of EcoStruxure Operator Terminal Expert v3.2 SP1+ (HMIEELCZLSPAZZ) for the configuration software. Note that the Professional License for EcoStruxure Operator Terminal Expert will also work if you already have it.
  2. The Physical HMIST6/HMISTM6 (Part Numbers: HMIST6200, HMIST6400, HMIST6500, HMIST6600, HMIST6700, HMISTM6200, or HMISTM6400)
  3. One WebViewer License (HMIWRT001)

For HMISTM6BOX, the WebViewer license is built-in and does not require a purchased WebViewer License, so what is needed is just:

  1. Basic License of EcoStruxure Operator Terminal Expert v3.2 SP1+ (HMIEELCZLSPAZZ) for the configuration software. Note that the Professional License for EcoStruxure Operator Terminal Expert will also work if you already have it.
  2. The Physical HMIST6400

For a Standard PC or Schneider Electric branded iPC, the requirements would be:

  1. Professional License for EcoStruxure Operator Terminal Expert v3.2 (HMIPELCZLSPAZZ). Note that the Basic License does not cover configuration of a Windows PC/iPC, the Professional License is required.
  2. A physical generic Windows 10 PC or Schneider Electric branded iPC running Windows 10
  3. One EOTE Runtime License for Windows (HMIRTWCZLSPAZZ)
  4. One WebViewer License (HMIWRT001)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: