undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use the topology settings in somove to change the ATV660 family to an ATV630 family?

Issue:

How can you convert a somove file with an ATV660 over to an ATV630 file?

Product Line:

ATV660, ATV680, ATV960, ATV980, ATV630 and ATV930

Environment:

All

Cause:

Files are not compatible across product families.

Resolution:

It’s not possible to do so. It’s not possible to select another “range” of ATV600. So no you can not convert an ATV660 file over to an ATV630 Drive using somove.

Once you log into Somove and choose topology these ATV660 and other ATV6XX family options will be grayed out.

Schneider Electric Saudi Arabia