{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the power of the wireless transmitters such as the ZBRN1 and PowerTag Link ?

The maximum isotopically radiated power of the ZBRN1 transmitter are :

  • With its internal antenna: 9.8 dBm (10 mW)
  • With a ZBRA2 external antenna: 4.8dBm (3.02 mW)

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: