Search FAQs
Does Logo smart relay from Siemens communicate with a Harmony HMI?
Issue:
Looking for a driver in VIjeo Designer or EcoStruxure Operator Terminal Expert that can communicate to LOGO! Smart Relay from Siemens
Product Line:
Harmony, Magelis, Vijeo Designer, EcoStruxure Operator Terminal Expert
Resolution:
Today, none of the Harmony or Magelis HMI's are able to communicate to a Siemens LOGO! Smart Relay. We currently only support communication to Siemens LOGO! PLCs. The recommendation is to verify with Siemens if the smart relay is able to communicate with Modbus TCP/IP or Modbus RTU. If so, then our HMIs could use the Modbus protocol to communicate to this relay.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: