{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to monitor Altivar, Altivar Process and Altivar Machine Drives for Motor Amp draw via Modbus RTU

Issue:

Can you monitor the motor Current using an Altivar ATV340 and Modbus RTU?

Product Line:

Altivar, Altivar 340 and Altivar Process Drive

Environment:

All models Altivar 340, ATV340

Resolution:

Yes, you would monitor Logic Address 3204 [LCr] Load Current via Modbus RTU

Schneider Electric Saudi Arabia