{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you set up the ATV630 drive to use the HMI in local when using ethernet IP assemblies 20 and 70?

Issue:

HMI in local when using ethernet IP assemblies 20 and 70?

Product Line:

ATV630 with the VW3A3720 option card.

Environment:

All

Cause:

Wants to use the HMI for command and speed in Local and remote is Ethernet IIP assemblies 20/70

Resolution:

Note you will need to be connected to Somove software to configure the drives settings.

First set up your Slot A Ethernet option card with the IP address, subnet etc. Choose Ethernet IP, Choose Assemblies 20/70 and check green check mark to confirm.

Somove ethernet ATV630 settings

Now you have to go into your Command and Reference menu and set up your command and references exactly like it is shown below.

ATV630 command settings

Now go back to your Slot A option card and choose Protocols and Drive profile and make sure it still shows assemblies 20 and 70 and then check he green check at the bottom.

Done.

Schneider Electric Saudi Arabia